Typically, you will not need to define allowable values in Measurement Locations where the ML Type field contains the value Numeric because the actual readings recorded against that checkpoint are likely to vary too much. For instance, for a Temperature Check, you might want users to enter the exact temperature, and you would not configure a list of allowable values.
For certain numeric readings, however, you might want to limit the user's choices to match the values that will be valid, if this is a limited range of values. For example, if a tank has level markings in eighths (0, 1/8, 1/4, 3/8, etc.), you could limit the valid choices to the numeric values 0, 0.125, 0.25, 0.375, etc.
Allowable values are stored in the Rounds Allowable Values family. Each record contains a value, the category of each value, and type of each value. The value in the record represents a value that will be available in a list on the device.
To completely configure a list of values for device users, you will need to:
- Create the necessary Rounds Allowable Values to store the values that will be available in the list.
- Select the values in the Allowable Values list in the Measurement Location representing the checkpoint at which users will need to select a reading value.
For example, suppose device users need to check the general condition of a pump, and you want them to select one of the following values: Leak, Motor Temp. High, Noise, OK, or Vibration.
To configure this list of values, you would need to create one Rounds Allowable Value record for each of the acceptable values, as shown in the following image.
Note: The type and category for each record is the same. Only the value varies from one record to the next.
In addition, you would need to create a Measurement Location and select the following values in the following fields.
Field |
Value |
ML Type
|
Character |
Category
|
Pump Check |
Allowable Values
|
Leak, Noise, Motor Temp. High, Vibration, and OK. |
The Allowable Values can then be selected in the Limit Values tab of the Measurement Location data sheet to define whether an alert will be displayed to the user of the mobile device, as shown in the following image: