Copy a Root Cause Analysis

This topic describes how to copy an analysis. You can also create a Root Cause Analysis from the RCA Overview page or create an analysis using the RCA Templates.

Steps

  1. Access the RCA Overview page.

  2. Select one of the following tabs:

    A list of available analyses appears based on the tab that you selected.

    The list of RCAs

  3. Select the row that contains the Root Cause Analysis that you want to copy.
  4. In the upper-right corner, select .

    The Copy Analysis dialog box appears, asking you to confirm that you want to create a new Root Cause Analysis based on the selected Root Cause Analysis.

  5. Select Yes.

    The Analysis Summary workspace appears in a new tab, displaying a blank datasheet for the new Root Cause Analysis.

    The blank datasheet of an RCA

  6. As needed, enter values in the available fields.
  7. Select .

    The new Root Cause Analysis is created and saved. The list of analyses on the RCA Overview page is updated.

Results

When you copy a Root Cause Analysis, any of the following items that exist in the original Root Cause Analysis will be copied to the new Root Cause analysis:

Copyright © 2018 General Electric Company. All rights reserved.