RCA Analysis records store basic information about a Root Cause Analysis created to track and analyze causes of Asset failures. The following table provides an alphabetical list and description of the fields that exist for the Root Cause Analysis family and appear by default on the RCA Analysis, RCA Analysis Summary, and Plant & Equipment Info datasheets. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior |
---|---|---|---|
Acknowledgments | Text | People who contribute to the analysis but are not members of the RCA team. |
You can enter a list of people who are not members of the RCA Team but who contributed expertise to the root cause analysis. For example, you may want to include the name, position, and company of each person who contributed to the development of the hypotheses, root cause, and recommendations for the pump failure that was analyzed. |
Analysis Name |
Character |
A value that identifies the Root Cause Analysis throughout the GE Digital APM product. |
This is a required field, and it must be unique. |
Analysis Type |
Character |
The type of RCA you are conducting. |
This field contains a list of the following values:
You can select the value that defines the type of analysis you are performing. This field is available on the RCA Analysis and RCA Analysis Detail datasheets. |
Asset Category |
Character |
The category of equipment associated with the RCA. |
You can enter a value in this field to describe the Asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet and is labeled Equipment Category. |
Asset Class |
Character |
The class of equipment associated with the RCA. |
You can enter a value in this field to describe the Asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet and is labeled Equipment Class. |
Asset Type |
Character |
The type of equipment associated with the RCA. |
You can enter a value in this field to describe Asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet and is labeled as Equipment Type. |
Charter |
Text |
The purpose of and requirements associated with conducting the RCA. |
You can enter a value in this field to describe the goal that the RCA Team wants to achieve by conducting an RCA. This value is populated automatically with the charter that you entered in the Team Charter section of the RCA Application Settings. |
Comments |
Text |
Any additional information about the current analysis. |
You can enter comments in this field. |
Cost |
Number |
The estimated cost of the failure event(s) you are analyzing. By default, the currency is set to $. |
You can enter a value in this field to specify the estimated cost. |
Date Published |
Date |
The date on which the RCA was published. |
This field is disabled. When the RCA is published, this field is updated automatically with the published date. |
Division |
Character |
The division of the equipment on which the RCA is being performed. |
You can enter a value in this field to describe the piece of equipment identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet. |
End Date |
Date |
The end date of the analysis, if applicable. |
You can select a date using the Calendar tool. The date specified in the End Date field must be greater than the date specified in the Start Date field. |
Event Narrative |
Text |
Information about the equipment failure. |
You can enter a description of the event in this field. |
Frequency |
Number |
The number of times the equipment failure occurred. |
You can enter a value in this field. |
Long Description |
Text |
A brief description of the current RCA. |
You can enter text in the Analysis Description dialog box. This field is labeled Analysis Description on the datasheet. |
Manufacturer |
Character |
The manufacturer of the piece of equipment on which you are performing the analysis. |
You can enter a value in this field to describe the manufacturer of the Asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet. |
Mechanism | Text | A brief description of the findings from the analysis. |
This field appears on the RCA Communicate datasheet and is labeled Summary of Findings. |
Plant Location |
Character |
The plant where the equipment failure occurred. |
You can enter a value in this field to describe the plant location of the asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet. |
Start Date |
Date |
The start date of the analysis. |
You can select a date using the Calendar tool. |
Unit |
Character |
The ID of the unit containing the piece of equipment for which you are conducting the RCA. |
You can enter a value in this field to describe the unit of the asset identified in the Asset ID field. This field appears on the Plant & Equipment Info datasheet. |
Copyright © 2018 General Electric Company. All rights reserved.