The Assets subsection contains information about the Asset records that are linked to the RCA Analysis record. The following image shows an example of the Assets subsection of the PROACT® RCA Analysis-At-A-Glance Overview section for the example RCA.
The following table lists each item in the Assets subsection and the corresponding record field whose data is displayed in the report.
Report Item | Record Family | Record Field |
---|---|---|
Record ID |
Equipment or Functional Location |
Equipment ID or Functional Location ID Note: This column contains the Record ID of each Equipment or Functional Location record that is linked to the RCA Analysis record. |
Family |
None |
Note: This field is populated automatically with the name of the family to which the piece of equipment or location belongs. If it belongs to the Equipment family, this field will be populated automatically with Equipment. If it belongs to the Functional Location family, this field will be populated automatically with Functional Location. |
Copyright © 2018 General Electric Company. All rights reserved.