The Risk Analysis Mapping family defines the Policy records that are used to populate the RBI Risk Matrix automatically from RBI Analyses. The following table provides the baseline state and behavior of fields that exist in the Risk Analysis Mapping family.
Note: The Risk Analysis Mapping family supports RBI Criticality, RBI Pipeline, and RBI PRD Criticality Analyses. These mappings support both the default and the Standard Practice risk matrices.
Field | Caption | Data Type | Description | Behavior and Usage |
---|---|---|---|---|
MI_RRSKMAP_ANLY_FAM_C | Analysis Family | Character | The Family ID of the analysis. | This field is populated automatically. |
MI_RRSKMAP_DEG_MECH_C | Degradation Mechanism | Character | The Degradation Mechanism that stores values that are used to populate the Risk Matrix. | This field is populated automatically. |
MI_RRSKMAP_POLICY_NM_C |
Policy Name | Character | The name of the Policy that is used to populate the Risk Matrix. | This field is populated automatically. |
MI_RRSKMAP_RISK_CTG_C | Risk Category | Character | The Risk Category that is populated on the Risk Matrix (e.g., Environment, Financial Risk, Operations, Safety). | This field is populated automatically. |
The Policy Input Nodes that are used by the Risk Analysis Mapping family to populate the RBI Risk Matrix depend on both the type of Risk Category that you choose and the Degradation Mechanism that you apply to the family. The information in the following tables indicates which policy nodes and input fields are used when populating your selected RBI Risk Matrix.
Note: When you calculate an RBI Criticality Analysis or RBI Pipeline Analysis, the Failure Frequency field is populated by Degradation Mechanism Evaluation that corresponds to each Degradation Mechanism in the selected RBI Analysis.
The following table provides the range of the financial loss based on the consequence category.
Consequence Category | Description | Range in USD |
---|---|---|
A | Catastrophic | > $10,000,000 |
B | Very Serious | $1,000,000 - $10,000,000 |
C | Serious | $100,000 - $1,000,000 |
D | Significant | $10,000 - $100,000 |
E | Minor | < $10,000 |
The value in the Production Loss Category field in a Criticality Consequence Evaluation indicates the amount of financial loss expected from an event. By default, the value in the Production Loss Category field is converted to a numeric equivalent, and mapped to the Production Loss input node in the risk mapping policies. The lowest value in each range is the default production loss value. The following table provides the default value of production loss based on the value in the Production Loss Category field.
Production Loss Category | Default Production Loss Value in USD |
---|---|
A | $10,000,000 |
B | $1,000,000 |
C | $100,000 |
D | $10,000 |
E | $5,000 |
Copyright © 2018 General Electric Company. All rights reserved.