A PRD Analysis for a pressure relief device can be created once you have identified at least one piece of equipment or RBI Component that it protects. PRD Analyses function the same way as RBI Analyses.
However, the following features that are available for RBI Analyses are not available for RBI PRD Analyses:
- Creating What If Analyses from RBI PRD Analyses
- Copying RBI PRD Analyses
- Specifying that TM Analysis values at the TML Group level be used to calculate RBI corrosion rate values
When you create a Criticality Calculator PRD Component: