Add a What-If Analysis

You can add a What-If Analysis to the following types of analyses:

When you create a What-If Analysis, a copy of the main RBI Analysis is created. In the What-If Analysis, however, the value in the Event Type field is populated with the value W.

You cannot add a What-If Analysis to an RBI PRD Criticality Analysis.

Steps

  1. Perform one of the following sets of steps:
    1. Access the analysis to which you want to add a What-If Analysis.

    2. In the upper-right corner of the workspace, select , and then select Create What If Analysis.

    -or-

    1. Access the component that is linked to the analysis to which you want to add a What-If Analysis.

      Below the graph, a list of analyses linked to the component appears in a grid.

    2. Select the check box that corresponds to the analysis to which you want to add a What-If Analysis.
    3. In the upper-right corner of the grid, select .

    The Create What If Analysis window appears.

  2. In the Create What If Analysis window:
  3. Select Done.

    The What-If Analysis is created and linked to the main analysis. The Analysis workspace appears, displaying the Analysis Details section.

    Note: If needed, modify values in the available fields, and then select to save your changes.

Results

Copyright © 2018 General Electric Company. All rights reserved.