The Design workspace appears, and the Select a Family or Query window is active, where you can add sources to the design canvas. After adding a source, you can use the design canvas to add fields to the grid in the Conditions section and to add criteria to the query.
The Select a query from the catalog window appears.
On the left side of the window, navigate to the folder that contains the query you want to view. Select the query, and then select Open.
The Results workspace appears.
In the page heading, select Design.
The Design workspace appears, where you can add sources to the design canvas. Use the design canvas to add fields to the grid in the Conditions section. Use the Conditions section to add criteria to the query.