Add a Field to a Query

Steps

  1. Access the Design workspace.
  2. In the design canvas, select the source that contains the field you want to add to the conditions grid.

    The [<Source Name>] window appears, where <Source Name> is the name that appears on the query source node in the design canvas.

    Query Add Field

  3. In the [<Source Name>] window, in the Fields section, select the field that you want to add to the query.

    The field appears in the grid in the Conditions section.

    Note: If you add the same field from one source to the grid in the Conditions section twice, you must specify a unique value in the Alias cell for each field. If you do not specify a unique alias, GE Digital APM will add a unique alias automatically.

Results

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.