Validate Policy Logic Using Policy Instance Values

You can validate the policy model logic using ad hoc test values or values in the records belonging to a policy instance. This topic describes how to validate the policy logic using values in the records belonging to a policy instance.

Steps

  1. Access the policy that you want to validate.

  1. At the bottom of the Design workspace, select the Validation tab.

    The Validation pane appears.

  1. On the left side of the pane, select the policy instance whose values you want to use in the validation process.

    The right side of the pane displays values from the records that are included in that policy instance. For example, in the following image, you can see that the value A is stored in the Criticality Indicator field in the Equipment record that is included in the policy instance.

  1. Select .

    The validation process begins. When the validation is complete, the nodes in the policy model are color-coded to indicate the results of the validation.

  1. In the policy model, select a node to view additional details about the specific node's execution.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.