A Rule node represents an action to execute a custom rule that provides functionality that the existing nodes in Policy Designer do not provide.
The inputs and outputs of a Rule node are defined by a rule that will be executed when the policy is executed.
IMPORTANT: The improper implementation of a rule through the Rule node could severely impact the performance of policy executions. If you want to use this node, you should contact GE Digital for additional instructions and assistance.
The Properties window for a Rule node contains the items that are described in the following table.
Item |
Description |
Notes |
---|---|---|
Rule Path text box |
Specifies the Catalog path to the rule project that contains the rule that will be executed when the policy is executed. |
You
can enter the path manually, or you can browse to it by selecting
the |
Rule Class list |
Specifies the class containing the specified rule. |
None |
Additional sections corresponding to the inputs defined by the specified rule. | Specifies the values for the inputs defined by the rule. | You can select |
Copyright © 2018 General Electric Company. All rights reserved.