A Last node is a Calculation node that you can use in a policy model to retrieve the last row in a collectionA set of results from a Query node or a set of readings associated with input nodes such as Measurement Location, Health Indicator, or OPC Tag., whose fields you can then use in successor nodes to perform various calculations or actions.
Note: For reading collections that are associated with Measurement Location, Health Indicator, or OPC Tag nodes, the last row is the most recent reading. For collections that are associated with Query nodes, the last row depends on the order in which the query is sorted.
The input for a Last node must be a collection. The output for the Last node is any field in the row that the Last node retrieves.
Copyright © 2018 General Electric Company. All rights reserved.