An Is Null node is a Calculation node that you can use to specify a default value that should be used in subsequent calculations in the event that the input value is null. You can also use this node in combination with a logic node to specify an action to be taken in the event that an input value is null.
The input of an Is Null node must be a single value. The output of an Is Null node, Answer represents either of the following two values:
Node Properties
The Properties window for an Is Null node contains the items that are described in the following table.
Item |
Description |
Notes |
---|---|---|
Input Value section |
Specifies the value that you want to determine whether it is null. |
You can select |
Value if Input is Null section |
Specifies the output value of the node if the value specified in the Input Value section is null. |
You can select |
Copyright © 2018 General Electric Company. All rights reserved.