A Create Production Event node
represents an action to create a
The outputs of the Create Production Event node are the following system fields for the record that the node creates: Content GUID, Entity KeyThe Entity Key output can be used in subsequent action nodes, such as the Create Relationship node, but will return a value of 0 if used in a calculation or a Return Value node, since the Entity Key is not available until the record is saved at the end of policy execution., Entity ID, and Site Key.
The Properties
window for a Create Production Event node contains the items that are described
in the following table. In each section, you can select the
Item |
Description |
Notes |
---|---|---|
Causing Asset Key section | Specifies the Equipment record that represents the piece of equipment that caused the event. |
The Causing Asset Key value must match exactly the Entity Key of the asset that caused the event. |
Description section |
Specifies a detailed description of the event. |
None |
End Date section |
Specifies the date that the event ended. |
Along with the start date, the end date determines whether or not the production event will be available in the Production Event list in the Production Event workspace. |
Headline section |
Specifies a short description of the event. |
None |
Source Production Unit section | Specifies the production unit to which loss is attributed. | The created Production Event record will be automatically linked to the specified Production Unit record. |
Start Date section | Specifies the date that the event started. | Along with the end date, the start date determines whether or not the production event will be available in the Production Event list in the Production Event workspace. |
Note: If you add a custom field to the Production Event family, that field will also appear in the Properties window for the Create Production Event node.
Hint: Click here to see an example of the Create Production Event node used within a complete policy model.
Copyright © 2018 General Electric Company. All rights reserved.