If
you copy a node that contains a mapped field value from another node,
the mapped field value will not be copied unless you also copy the node
from which the values are mapped and the connector node between the two
nodes.
Connections will be copied only if
you select the connection and both nodes that it connects.
After
you paste a node that requires a unique name (e.g., Point Value node),
you must change the name of the copied node before you can save the policy.
You cannot copy nodes and connections from one policy to another.
Steps
Access the policy containing the nodes that you want to copy and paste.
In the Design
workspace, on the model canvas, press the Ctrl key and select all
the nodes and connections that you want to copy.
Hint: You can press Ctrl + A to select all nodes and connections in the policy model.
The selected nodes and connections are outlined
in blue, as shown in the following image.
In the Edit section of the
toolbar, select .
The selected nodes and connections are copied.
In the Edit section of the toolbar, select .
Copies of the selected nodes and connections are
pasted to the model canvas and are selected automatically.
Drag the pasted nodes and connections to a new location as necessary.