Consider the following nodes and connections.
In this example, the A Constant
node is connected to a successor Condition node. This Condition node is
also connected to another predecessor node, which is an Entity node representing
the Equipment family.
As shown in the following image, you can use the Properties
window for the Condition node to select the AConstant node and its value, which is A. With these options selected, the Condition node evaluates
whether or not the value in the Criticality Indicator field of a specified Equipment record is A.
Regardless of the Equipment records specified via policy instances, the Condition node will always compare the value in the Criticality Indicator field to A.