The following tables outline the steps that you must complete to upgrade this module to
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
This module will be updated to
Step | Task | Notes |
---|---|---|
1 | Replace the Top 10 Bad Actors query for the PLA Overview page. |
This step is optional. The Top 10 Bad Actors query is used by GE Digital APM to populate the Top 10 Bad Actors graph on the Production Loss Analysis Overview page. In some databases, when viewing this graph, you may receive an error that prevents the graph from populating correctly. If this error occurs, then replace the Top 10 Bad Actors query. |
Step | Task | Notes |
---|---|---|
1 | Replace the Top 10 Bad Actors query for the PLA Overview page. |
This step is optional. The Top 10 Bad Actors query is used by GE Digital APM to populate the Top 10 Bad Actors graph on the Production Loss Analysis Overview page. In some databases, when viewing this graph, you may receive an error that prevents the graph from populating correctly. If this error occurs, then replace the Top 10 Bad Actors query. |
Step | Task | Notes |
---|---|---|
1 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.6.0.0.0. |
2 | Set the timezones for the Production Units. |
This step is required. If the timezones for the Production Units are set, all the Production Plan records, Plan Data records, and Production Target records will be updated based on the timezone for the respective Production Unit. Note: Since the date and time in PLA is now stored in UTC format, you must set the timezone for each Production Unit before upgrade.
|
Step | Task | Notes |
---|---|---|
1 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.6.0.0.0. |
2 | Set the timezones for the Production Units. |
This step is required. If the timezones for the Production Units are set, all the Production Plan records, Plan Data records, and Production Target records will be updated based on the timezone for the respective Production Unit. Note: Since the date and time in PLA is now stored in UTC format, you must set the timezone for each Production Unit before upgrade.
|
Step | Task | Notes |
---|---|---|
1 | On the GE Digital APM Server, import the required baseline rules. |
IMPORTANT: This step is required and must be completed before upgrading the GE Digital APM Server and Add Ons software on GE Digital APM(s). After completing this step, you should return to the upgrade GE Digital APM workflow. Then, after completing the remainder of the upgrade GE Digital APM workflow, when you are ready to upgrade PLA, proceed to step 2 in this workflow. |
2 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.5.1. |
Step | Task | Notes |
---|---|---|
1 | On the GE Digital APM Server, import the required baseline rules. |
IMPORTANT: This step is required and must be completed before upgrading the GE Digital APM Server and Add Ons software on GE Digital APM(s). After completing this step, you should return to the upgrade GE Digital APM workflow. Then, after completing the remainder of the upgrade GE Digital APM workflow, when you are ready to upgrade PLA, proceed to step 2 in this workflow. |
2 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.5.0. SP1 LP. |
Step | Task | Notes |
---|---|---|
1 | On the GE Digital APM Server, import the required baseline rules. |
IMPORTANT: This step is required and must be completed before upgrading the GE Digital APM Server and Add Ons software on theGE Digital APM(s). After completing this step, you should return to the upgrade GE Digital APM workflow. Then, after completing the remainder of the upgrade GE Digital APM workflow, when you are ready to upgrade PLA, proceed to step 2 in this workflow. |
2 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.5.0. |
Step | Task | Notes |
---|---|---|
1 | On the GE Digital APM Server, import the required baseline rules. |
IMPORTANT: This step is required and must be completed before upgrading the GE Digital APM Server and Add Ons software on GE Digital APM(s). After completing this step, you should return to the upgrade GE Digital APM workflow. Then, after completing the remainder of the upgrade GE Digital APM workflow, when you are ready to upgrade PLA, proceed to step 2 in this workflow. |
2 | Define OEE codes. | This step is required only if you want to use custom OEE Code records instead of or in addition to the baseline OEE Code records that are provided in the GE Digital APM database. If you do, you will need to create custom OEE codes to identify the types of losses you can incur. Each OEE code will be stored in an OEE Code record. |
3 | Define values that will be mapped to a Production Analysis. | By default, certain PLA values are mapped to the production data in a Production Analysis. This step is required only if you want to map different or additional PLA values. If you do, you will need to modify the All Production Data query. |
4 | Confirm the deployment of the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server. | This step is required only if you did not deploy the Production Data cube and Equipment Costs Data cube on the SQL Server Analysis Server in V3.4.5. |
Related Information
Copyright © 2018 General Electric Company. All rights reserved.