The following tables outline the steps that you must complete to upgrade this module to
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
When you upgrade:
Step | Task | Notes |
---|---|---|
1 |
Uninstall the previous version of the Meridium Device Service, and install the latest version on all the machines that you will connect to a device used for automated calibration. IMPORTANT: If, however, you use HTTPS to connect to GE Digital APM, then you must follow the instructions in KBA 2850. |
This step is required only if you want to use a device to perform automated calibration. |
2 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade:
Step | Task | Notes |
---|---|---|
1 |
Uninstall the previous version of the Meridium Device Service, and install the latest version on all the machines that you will connect to a device used for automated calibration. IMPORTANT: If, however, you use HTTPS to connect to GE Digital APM, then you must follow the instructions in KBA 2850. |
This step is required only if you want to use a device to perform automated calibration. |
2 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade:
For each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Uninstall the previous version of the Meridium Device Service, and install the latest version on all the machines that you will connect to a device used for automated calibration. IMPORTANT: If, however, you use HTTPS to connect to GE Digital APM, then you must follow the instructions in KBA 2850. |
This step is required only if you want to use a device to perform automated calibration. |
2 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade:
For each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Uninstall the previous version of the Meridium Device Service, and install the latest version on all the machines that you will connect to a device used for automated calibration. IMPORTANT: If, however, you use HTTPS to connect to GE Digital APM, then you must follow the instructions in KBA 2850. |
This step is required only if you want to use a device to perform automated calibration. |
2 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade:
For each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade:
For each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade, for each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade, for each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
When you upgrade, for each Calibration record whose Calibration Closed check box is selected, the state is changed to Approved.
Step | Task | Notes |
---|---|---|
1 |
Using the command prompt, navigate to the <GE Digital APM installation folder>/Upgrade folder, and then run the following command: Meridium.DbUtility.CalibDeviceMappingsUpgradeUtility.exe <datasource ID> <username> <password>
Where,
|
This step is required only if you want to use the Fluke documenting process calibrator. This will replace the old Calibration Device Mappings for the device with the new ones. It will also update the existing templates to use the new Calibrator Device Mappings. After you complete this step, a log file is generated containing information about the upgrade process. |
Related Information
Copyright © 2018 General Electric Company. All rights reserved.