IMPORTANT: You must repeat this procedure on each machine to which you will connect a calibrator.
The Meridium Device Service can be installed as part of the workflow when you try to send data to a calibrator or verify the settings of the calibrator.
Steps
Access the Calibration Management Overview page.
Note: A calibrator does not need to be connected.
Select the Calibration Tools tab.
The Calibration Tools section appears, displaying a list of test equipment and standard gas cylinders.
In the upper-right corner of the page, select Calibrator Settings.
The Calibrator Settings window appears.
In the Select Device box, select the required device.
If you selected the CMX Calibration Management software, enter values in the following fields:
In the Device Service Settings Service Port box, enter the value of the service port number that you have configured. The default value in the Device Service Settings Service Port box is 2014.
If you selected a Fluke documenting process calibrator, enter values in the following fields:
In the COM Port box, select the communication port number to which the calibrator is connected.
IMPORTANT: GE Digital APM supports port numbers in the range of COM1 through COM4. If the communication port number of the calibrator does not fall within this range, you must change the value in the Device Manager, or connect the calibrator to a different port.
If you want to test the connection of the Fluke documenting process calibrator, select the Perform Connection Test check box.
Note: The Baud Rate box contains the value 9600. You cannot change this value.
In the Device Service Settings Service Port box, enter the value of the service port number that you have configured. The default value in the Device Service Settings Service Port box is 2014.
If you selected a GE Druck documenting process calibrator, enter values in the following fields:
Select Done.
The Calibrator Settings window appears, indicating that the Meridium Device Service is not installed.
Select Download.
The file MeridiumDevices.exe is downloaded.
Run MeridiumDevices.exe, and then follow the instructions in the installer.
The Meridium Device Service is installed.
Copyright © 2018 General Electric Company. All rights reserved.