This topic describes how to send Calibration data to a calibrator when performing an automated calibration.
IMPORTANT: In Fluke 74x-75x, you can perform automated calibration only if the user ID that you enter in the calibrator belongs to one of the Security Users in GE Digital APM. Refer to the calibrator documentation for instructions on how to enter the user ID in the calibrator.
Steps
Access the Calibration Management Overview page.
Hint: You can also access the Calibration Management Overview page for a hierarchy level.
Select the Calibration Queue tab.
The Calibration Queue section appears, displaying a list of calibration queue records.
In the row for each calibration queue record that you want to send to the calibrator, select the check box.
In the upper-right corner of the section, select Send for Calibration.
The Send for Calibration window appears, displaying the Select Calibration Method section.
In the Send To box, select the calibrator type that you want to use for calibration. You can select one of the following options:
Druck DPI620G (Genii) (Druck DPI620G – Advanced Multifunction Calibrator, HART/Fieldbus Communicator)
If you want to send the data to a Fluke documenting process calibrator, select Fluke 74x – 75x.
In the Calibrator Device ID box, select the device ID of the calibrator.
Note: If you have selected CMX, the Calibrator Device ID box will be disabled.
The calibration driver details, device details, and certification details for the selected device appear.
Note: If you have not verified the calibrator settings, an error message appears below the Send To box, stating that the settings for this device have not been configured and the Next button will be disabled. If this occurs, you must verify the settings.
In the lower-right corner of the window, select Next.
Note: If a test equipment for the selected device has not been created, the Next button will be disabled and a validation message will appear, indicating that the test equipment for the device has not been found and that you need to create a test equipment before proceeding.
The Validate Selection section appears, displaying, the list of calibration applied templates that are compatible with the device that you selected.
Note: If the selected calibration queue records have not been mapped to the correct device, when you select Next, the Calibration Templates will not be loaded and the Finish button will be disabled.
Select Finish.
The Sending to Calibrator section appears, displaying the progress of sending the data to the calibrator. The Send completed message indicates that the data has been sent to the calibrator.
Note: If the Meridium Device Service is not installed or not running, an error message appears, indicating that the Meridium Device Service could not be reached. The message also indicates that you need to verify that the service is installed and running. You can select the Download link to download the installer. After the service is running, select Continue to send the data to the calibrator.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.