License Requirements
The Calibration license is required to take advantage of the Calibration Management functionality.
Additional Components Required
If you use a documenting process calibrator or other calibration management software to perform automated calibration, then the machine that will connect to that calibrator must have the GE Digital APM Devices service installed.
These devices may require additional drivers provided by the manufacturer.
The following documenting process calibrator devices are supported:
Druck DPI611 - Pressure Calibrator
Druck DPI612 - Flex Pressure Calibrator
Druck DPI620 - Multifunction Calibrator
Druck DPI620-IS - Intrinsically Safe Multifunction Calibrator
Druck DPI620G – Advanced Multifunction Calibrator, HART/Fieldbus Communicator
Druck DPI620G-IS - Intrinsically Safe Advanced Multifunction Calibrator, HART/Fieldbus Communicator
The following Calibration Management software is supported:
To establish communication with the CMX Calibration Management software, in addition to GE Digital APM Device services, you must install the following software:
Deploying Calibration Management
After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for Calibration Managaement.
Supported Features in
All standard GE Digital APM product features for this module are available in the
Copyright © 2018 General Electric Company. All rights reserved.