Steps
On the Windows Mobile handheld device, open Internet Explorer, and navigate to the URL http://<machine>/MeridiumSyncService, where <machine> is the name or IP address of the server on which APM Sync Services is installed.
You are redirected automatically to one of the following URLs, and then a download screen appears:
If the device is running Windows Mobile 2003, select PPC2003\NETCFv35.PPC.ARMV4.CAB.
or
If the device is running Windows Mobile 5.0 or later, select WCE500\NETCFv35.WM.ARMV4i.CAB.
A message appears, asking if you really want to download the file.
Select Yes.
The file is downloaded, and the .NET Compact Framework is installed. When the installation is complete, a message will appear indicating that the installation is successful and instructing you to restart the device.
Copyright © 2018 General Electric Company. All rights reserved.