Steps
On the Windows Mobile handheld device, open Internet Explorer, and then navigate to the URL http://<machine>/MeridiumSyncService, where <machine> is the name or IP address of the server on which APM Sync Services is installed.
You are redirected automatically to one of the following URLs, and then a download screen appears:
Select MFX.APM.<version>.ARM4.CAB, where <version> is the corresponding version of GE Digital APM.
A message appears, asking if you really want to download the file.
Select Yes.
The file is downloaded, and the APM Mobile Framework is installed. When the installation is complete, a message will appear, indicating that the installation is successful.
The APM Mobile Framework screen appears, indicating that no users are available on the Windows Mobile device yet.
Copyright © 2018 General Electric Company. All rights reserved.