The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Note: This GE Digital APM module is not available in the APM Now environment.
Step |
Task |
Notes |
---|---|---|
1 |
Assign Security Users to one or more of the GE Analytics Security Groups and Roles. |
This step is required. |
2 |
Modify the file Meridium.AMQP.Service.exe.config to configure the RabbitMQ connection. | This step is required. |
3 |
Restart the AMQP Service. | This step is required. |
4 | Install GE System 1 Integration Service. | This step is required. |
5 |
Create and configure the GE Connection record to connect to the GE Message Broker Server. |
This step is required. |
6 |
Modify the file Meridium.GE.Service.exe.config to configure the GE Service. |
This step is required. |
7 |
Configure the GE Service to restart automatically. |
This step is required. |
8 |
Start the GE Service. |
This step is required. Once the GE Service is started, the GE Enterprise hierarchy will import automatically into the GE Digital APM database. |
9 |
This step is required. These records are created automatically by the GE Service. |
|
10 |
Stop and then start the GE Service. |
This step is required. |
11 |
Link tags to assets (i.e., equipment and functional locations). |
This step is required. You must repeat this step for any GE Tags records that are imported from your GE system. New tags are imported automatically. |
12 |
This step is required only if you want to use GE policies. |
Copyright © 2018 General Electric Company. All rights reserved.