GE Analytics System Requirements

License Requirements

The GE System 1 Integration license is required to take advantage of the GE Analytics functionality.

Additional Components Required

In addition to the basic GE Digital APM system architecture, your system must also contain the following additional components:

Data from GE systems, such as GE System 1 and GE SmartSignal, is transferred to GE Digital APM via Enterprise Impact 17.1 SP1. This GE Fleet Message Server represents the following components:

Note: We recommend that these components be installed on the same machine to simplify the configuration of this module. However, in your system architecture, these components may be installed on separate machines.

System Architecture

The following image shows how the additional components should be incorporated into the basic GE Digital APM system architecture to support this module.

Deploying GE Analytics

After you have installed and configured the basic GE Digital APM system architecture, you will need to perform some configuration steps specifically for GE Analytics.

Supported Features in APM Now

This GE Digital APM module is not available in the APM Now environment.

Copyright © 2018 General Electric Company. All rights reserved.