Install the GE System 1 Integration Service

Steps

  1. On GE Enterprise Impact 17.1 SP1 Message Server, access the GE Digital APM distribution package, and then navigate to the folder \\Setup\Meidium Enterprise APM Server and Add-ons.
  2. Double-click the file Setup.exe.

    The Welcome screen appears.

  3. Select Next.

    The License Agreement screen appears.

  4. Read the License Agreement, and, if you agree, select the I accept the terms of the license agreement check box. Then, select Next.

    The Select Installation Location screen appears.

  5. Select Next to accept the default location.

    The Select the features you want to install screen appears.

  6. Select the Meridium GE System 1 Integration Service option.

    Note: While additional options are available for selection, these options are not meant to be installed on the Meridium Integration Service server. These instructions assume that you want to install only the Meridium Integration Service software. When this software is installed, the APM System Administration tool will also be installed automatically.

  7. Select Next.

    The Complete the Installation screen appears.

  8. Select Install.

    The Installation is Complete screen appears.

  9. Select Finish.

    The GE System 1 Integration Service is installed.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.