In the right corner of the Proof Test that you want to delete, select .
The Confirm Delete dialog box appears, asking you if you want to delete the Proof Test from the offline store.
Select Yes.
The selected Proof Test is deleted from the offline store.
Notes:
When you delete a Proof Test, the associated Proof Tests Details are also deleted from the offline store.
When you delete a Proof Test from the offline store, the related Proof Test will still be available in the GE Digital APM database. As needed, you can manually delete the Proof Test from the database.
Results
If the Proof Test that you deleted was associated with a Recommendation, then the Recommendation and any image associated with the Recommendation are deleted from the offline store.
If a Recommendation is associated with more than one Proof Test, and you deleted one of the Proof Test, then the Recommendation and associated images will not be deleted.