SIS Functional Test Detail Records

This topic provides an alphabetical list and description of the fields that exist in the SIS Functional Test Detail family. When you apply a Proof Test Template to a Proof Test, a Functional Test Detail is created for each Proof Test Template Detail. The values in most of these fields are populated with the values in the corresponding fields in the related Proof Test Template Detail. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

As Found Travel Time Numeric The time taken by the Final Element to reach the safe state from its normal operating state. This value is measured in seconds.

This field is enabled only if the value in the Step Type field is Final Element.

If the value in this field exceeds the value in the Travel Time Limit field, then the proof test step fails.

As Found Trip Point Numeric A number that defines when the element has activated an SIS shutdown.

This value is used to calculate the As Found Trip Point Error.

As Found Trip Point Error Numeric The error value calculated for the value that you have entered in the As Found Trip Point field.

This value is disabled and calculated as follows:

As Found Trip Point Error = [(As Found Trip Point - Trip Point) *100] / Trip Point

If this value is less than the value in the Trip Point Error Limit field, then the proof test step has passed. Otherwise, it has failed.

As Left Travel Time Numeric The time taken by the Final Element to reach the safe state from its normal operating state, after repairing the element. This value is measured in seconds.

This field is enabled only if the value in the Step Type field is Final Element.

As Left Trip Point Numeric A number that defines when the element has activated an SIS shutdown after repairing the element. This value is used to calculate the As Left Trip Point Error.
As Left Trip Point Error Numeric The error value calculated for the value that you have entered in the As Left Trip Point field.

This value is disabled and calculated as follows:

As Left Trip Point Error = [(As Left Trip Point - Trip Point) *100] / Trip Point

Comments Character Comments about the proof test.

None

Equipment ID

Character

The ID of the Equipment against which the step is performed.

This field is disabled and populated with the value in the Equipment ID field in the corresponding Proof Test Template Detail.
Executed By Character The ID of the user who conducted the proof test. This field is disabled and populated with the ID of the current user.
Execution Date Date The date on which the proof test was conducted. This field is disabled and populated with the date and time on which the Functional Test Detail is saved.
Failure Condition Character The condition in which the proof test step failed. None
Failure Type Character The type of the failure.

This field contains the following values:

  • Safe
  • Dangerous
  • No Effect
Location ID Character The ID of the Functional Location against which the step is performed. This field is disabled and populated with the value in the Location ID field in the corresponding Proof Test Template Detail.
Pass/Fail Character Indicates whether the proof test step has passed or failed based on the pass/fail criteria that you have specified in the corresponding Proof Test Template Detail.

This field contains the following values:

  • Pass
  • Fail
  • Skip
  • Complete
Result Criteria Text A description of what is considered to be an acceptable result of the step. This field is disabled and populated with the value in the Result Criteria field in the corresponding Proof Test Template Detail.
Step Sequence Number Numeric A number that represents the order in which the step should be performed, relative to other steps. This field is disabled and populated with the value in the Step Sequence Number field in the corresponding Proof Test Template Detail.
Step Type Character The type of the step. This field is disabled and populated with the value in the Step Type field in the Proof Test Template Detail.
Template Detail ID Character An alphanumeric value that identifies the SIS Functional Test Detail.

This field is disabled and populated with the value in the Template Detail ID field in the corresponding Proof Test Template Detail.

Test Criteria Character The criteria or conditions for conducting the proof test. This field is disabled and populated with the value in the Test Criteria field in the corresponding Proof Test Template Detail.
Travel Time Limit Numeric A number that quantifies the maximum acceptable travel time for this step, in seconds. This field is enabled only in SIS Proof Test Template Details that are linked to records representing final elements.
Trip Point Numeric A number that defines when the element should activate an SIS shutdown. This field is enabled only in SIS Proof Test Template Details that are linked to records representing sensors, final elements, or logic solvers.
Trip Point Direction Character The trend of Trip Point values. This field is disabled and populated with the value in the Trip Point Direction field in the corresponding Proof Test Template Detail.
Trip Point Error Limit Numeric A value that defines the range, plus or minus, within which the Trip Point value must fall to be acceptable. This field is disabled and populated with the value in the Trip Point Error Limit field in the corresponding Proof Test Template Detail.
Trip Point Units Character The unit of measure associated with the value in the Trip Point field. This field is disabled and populated with the value in the Trip Point Units field in the corresponding Proof Test Template Detail.

Copyright © 2018 General Electric Company. All rights reserved.