SIS Proof Test Records

SIS Proof Test records store details about a proof test that is executed, including the results of the proof test. This topic provides an alphabetical list and description of the fields that exist for the SIS Proof Test family and appear on the SIS Proof Test datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Cleared All Bypasses and Forced Logic

Logical

Indicates whether or not you have cleared all bypasses and forced logic while performing the proof test.

None

Commencement Date Date The date on which the proof test was started. None
Completion Date Date The date on which you completed the proof test. None
Equipment Operating State Character The current state of the equipment that you are testing.

This field contains the System Codes that exist in the MI EQUIP OP STATE System Code Table. You can choose from the following baseline values:

  • ON-LINE (ON-LINE)
  • Off-Line (OFF-LINE)
  • Not Applicable (NA)
Functional Test Closed Logical A value that indicates whether or not the proof test has been completed. If you select this check box, all fields on the SIS Proof Test datasheet are disabled.
Functional Test Status Character Stores the current status of the proof test.

This field contains the System Codes that exist in the MI FUNCTIONAL TEST STATUS System Code Table. You can choose from the following baseline values:

  • Active
  • Complete
  • Closed
Functional Test Template Character The ID of the SIS Proof Test Template that was used to create the SIS Proof Test. This field contains a list of proof test templates that are approved and linked to the instrumented function on which you are conducting the proof test. This field is required. After you select a template from the list and save the record, this field is disabled. The Proof Test Template Detail records linked to the selected template are listed in the Analysis Details section.
SIS Or PIF Key Numeric The Entity Key of the Instrumented Function or the Logic Solver to which the SIS Proof Test record is linked. This field does not appear on the datasheet by default.
SIS Tester Name Character The name of the user who is responsible for performing the proof test.

This field contains the names of:

  • The Security User who created the SIS Proof Test

-and-

  • Members of the MI SIS Administrator, MI SIS Engineer, or MI SIS User Security Groups
Task Addressed Numeric The inspection task that is addressed by the proof test. This field contains the inspection tasks that are linked to the instrumented function or the logic solver on which you have performed the proof test.
Test Description Character A description of the proof test. None
Test ID Character The ID for the proof test.

None

Test Summary Text A summary of the proof test that you have performed. None
Type of Test Character The type of the proof test that you have performed.

This field contains the following baseline values:

  • Functional Test
  • System Validation

Copyright © 2018 General Electric Company. All rights reserved.