The Maps module helps provide a visual companion to illustrate your data in a way that is dynamic and easy to understand.
The Maps module is built using the same SQL queries used throughout GE Digital APM to allow maximum flexibility.
The Baseline Map Query is located in the Catalog under \\Public\Meridium\Modules\Core\Queries\Map Queries.
The Baseline Map Query comes with five fixed columns:
Column | Parameter | Description |
---|---|---|
1 | Unique ID | The first column has a unique identifier for the information included in the Maps query. Typically, it is an Entity Key for a specific piece of data. |
2 | Functional Location | This column contains the functional location of the objects being mapped. |
3 | Region | This column contains the geospatial data for the value being mapped. |
4 | Color | This column contains the color value for the data that is being mapped. You can use either hex or RBG values. |
5 | Marker |
This column contains the value for the geospatial marker. This field is not case sensitive, and it can be any of several shapes, including:
|
Beyond the five baseline columns, there is no limit to the number of additional columns that can be added to the query.
Beyond the five baseline columns, any additional columns of information queried will appear on the visual map, on an inset window, when an entity is selected.
If a hyperlink is included on any additional columns beyond the five baseline columns, it will appear on the visual map, on an inset window, when an asset or location is selected.
Queries are highly flexible and incredibly customizable. For more information about how to use queries in GE Digital APM, refer to the documentation on queries.
Note: Please note that Maps will only load data sets with five hundred points or fewer on mobile devices.
Copyright © 2018 General Electric Company. All rights reserved.