Steps
Select the IPL Checklist tab.
The IPL Checklist section appears, displaying a set of criteria to identify if the Safeguard is an IPL.
In the IPL Checklist section, next to each criteria that is applicable for the selected Safeguard, select the check box.
The IPL Type box and the IPL Sub Type box are enabled.
Note: The IPL Type box and the IPL Sub Type box are enabled only if the check box for all the criteria in the IPL Checklist section is selected.
In the upper-right corner of the workspace, select
The Safeguard is specified as an IPL.
Results
Copyright © 2018 General Electric Company. All rights reserved.