Create a Safeguard

This topic describes how to create a Safeguard.

Note: You can create a Safeguard only if the associated LOPA is in the Planning state. Additionally, if the LOPA is linked to a Consequence in Hazards Analysis, you can create a Safeguard only if the Hazards Analysis is also in the Planning state.

Steps

  1. Access the Layer of Protection Analysis for which you want to create a Safeguard.
  2. In the left pane, select Safeguards and IPLs.

    The Safeguards and IPLs workspace appears, displaying a list of safeguards linked to the LOPA.

    List of Safeguards

  3. In the upper-left corner of the workspace, select

    A blank datasheet for the Safeguard appears, displaying the Definition section.

    Safeguard

  4. As needed, enter values in the available fields.
  5. In the upper-right corner of the workspace, select .

    The Safeguard is created and linked to the selected LOPA.

Result

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.