This topic describes how to create the following components of a hazards analysis using a blank datasheet:
You can also copy a Component.
Hint: You can create a Component only if the corresponding Hazards Analysis is in the Planning state.
Steps
Select the Hazards Worksheets tab.
The Hazards Worksheets section appears, displaying a hierarchical view of the components (Deviations or What Ifs, Causes, Consequences, and Safeguards) associated with the System/Node.
In the hierarchical level that corresponds to the component that you want to create, select
Where <type of component> can be one of the following values:
For example, if you want to create a new Deviation, then in the Deviations hierarchical level, select
A blank datasheet for the type of component appears.
In the upper-right corner of the datasheet, select
A new component is created and listed in the corresponding hierarchical level. For example, if you have created a new Deviation, it will be listed in the Deviations hierarchical level.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.