HAZOP Deviation records store details on the condition within a process that deviates from the normal behavior during that process, resulting in a risk. This topic provides an alphabetical list and description of the fields that exist for the HAZOP Deviation family. These fields appear on the HAZOP Deviation datasheet, unless otherwise specified. The information in this table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Deviation/Guideword |
Character |
A brief description of the deviation. |
This field contains the description of the System Codes that exist in the MI_HAZOP_DEVIATIONS_TYPE System Code table. You can choose from the following baseline values:
This value appears in the list of Deviations in the hierarchical view of the components of the System/Node. |
Deviation/Guideword Number |
Character |
A set of numeric values, separated by a decimal point, which represents the location in which the Deviation appears in the hierarchical view of the components of the System/Node. |
This field is disabled and populated with a set of numeric values, separated by a decimal point.
|
Sequence Number | Number | A numeric value that represents the sequence in which the Deviation appears in the hierarchical view of the components of the System/Node, relative to the other Deviations that are linked to the same System/Node. | This field does not appear on the datasheet by default. This value in this field is used to populate the Deviation/Guideword Number field. |
Copyright © 2018 General Electric Company. All rights reserved.