Hazards Analysis Consequence Records

Hazards Analysis Consequence records store details on the specific risk that is associated with a given scenario. This topic provides an alphabetical list and description of the fields that exist for the Hazards Analysis Consequence family. By default, these fields appear on the Hazards Analysis Consequence datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage

Consequence Comment

Text

Comments about the risk.

None

Consequence Description

Text

A detailed description of the risk.

None

Consequence ID Character A brief description of the risk. This is a required field.
Consequence Number Character A set of four numeric values, separated by a decimal point, which represents the location in which the Consequence appears in the hierarchical view of the components in the System/Node.

This field is disabled and populated with numbers, separated by decimal points (e.g., 2.1.1.1).

  • The first three numbers correspond to the value that exists in the Cause Number field in the Cause to which the Consequence is linked.
  • The fourth number is the value that exists in the Sequence Number field in the Consequence.
Consequence Type Character The type of risk.

This field contains the description of the System Codes that exist in the MI_HAZOP_CONSEQUENCE_TYPE System Code Table. You can choose from the following baseline values:

  • Fire
  • Explosion
  • Single Fatality
  • Multiple Fatalities
  • Equipment Damage
  • Production Loss
Sequence Number Number A numeric value that represents the position in which the Consequence appears in the hierarchical view of the components in the System/Node, relative to the other Consequences that are linked to the same Cause. This field is used to populate the Consequence Number field, and does not appear on the datasheet by default.

Copyright © 2018 General Electric Company. All rights reserved.