Access a Component

This topic describes how to access the datasheet of the following types of components of a hazards analysis:

Steps

  1. Access the System/Node that is linked to the component that you want to access.
  2. Select the Hazards Worksheets tab.

    The Hazards Worksheets section appears, displaying a hierarchical view of the components (Deviations or What Ifs, Causes, Consequences, and Safeguards) associated with the System/Node.

  3. Select the component that you want to access, and then, in the upper-left corner of the workspace, select .

    The datasheet for the selected component appears.

    The datasheet of a Deviation

  4. If needed, modify values in the available fields for Deviation, What If, Cause, Consequence, or Safeguard.

    Hint: You can modify a Component only if the corresponding Hazards Analysis is in the Planning state.

  5. In the upper-right corner of the datasheet, select .

    The changes made to the component are saved.

    Tip: You can select in the upper-left corner of the workspace to return to close the datasheet.

Copyright © 2018 General Electric Company. All rights reserved.