Modify a State

You can modify the properties of an existing state. For example, you can change the caption of a state Draft to Draft 1, mark an existing state as initial state, remove the roles assigned to a state, and so on.

Steps

  1. Access the State Configuration section.
  2. In the Manage State Configuration workspace, select the state that you want to modify.

    The Properties-<Label> window appears, where the <Label> is the name of the state that you want to modify.

  3. As needed, modify the available fields.
  4. To remove the assigned roles, in the Selected Roles box, select the role, and then select .

    The selected role is removed from the Selected Roles box.

  5. Select OK.

    The updated state appears in the workspace.

  6. Select Save.

    The state is modified.

 

Copyright © 2018 General Electric Company. All rights reserved.