Add a New State to a Family

When defining the State Configuration for a family, keep in mind the workflow that you want users to follow. Then, create states and operations that facilitate that workflow and decrease the possibility of error. After defining the workflow between the states, you can display the states on the datasheet and manually move the states defined in a workflow.

Steps

  1. Access the State Configuration section.
  2. Depending on your requirement:

    The Show States on Datasheets check box and the Add State button appears enabled.

  3. Select Add State to define a new state.

    The Properties-New State window appears.

  4. As needed, specify the values in the following fields:

  5. If you want the state to appear on the datasheet, select Show States on Datasheets check box.

    By default, the check box is selected. If you do not want the state to appear on the datasheet, clear the Show States on Datasheets check box, and then select Save.

    Note: You can now hide or show the state configuration on a datasheet for a subfamily, even if the state configuration is inherited from the parent family.

  6. For the Roles:

    Note: You can select to search for a role.

  7. Select OK.

    The Properties window closes and the new state appears on the workspace.

    State Configuration New State

  8. Select Save to save the State Configuration.

    Your changes are saved.

Copyright © 2018 General Electric Company. All rights reserved.