As needed, enter the values in the following fields:
ID: Delete the text that was generated automatically, and type an ID for the new operation.
Caption: The Caption box is populated automatically with the value that you typed in the ID text box. You can change the caption if desired.
Predecessor State: Select the state that should serve as the predecessor state, or the state from which this operation will transition a record. For example, if a record can go from Created to Assigned via the Assign operation, to add the Assign operation, you would need to select the Created state as the predecessor state.
Successor State: Select the state that should serve as the successor state, or the state to which this operation will transition a record. For example, if a record can go from Created to Assigned via the Assign operation, to add the Assign operation, you would need to select the Assigned state as the successor state.
Is Reserved: This option is available only for the baseline operation. If the operation is marked as Is Reserved, then you cannot delete that operation. You can, however, modify the Caption of the operation.