Access or Modify an Offline Form

Steps

  1. Access the Offline Form Builder.

    Note: If there is an existing offline form for the entity, the offline form for that entity appears. If there is more than one Offline form, the default offline form for that entity appears.

  2. To select an offline form, then in the upper-right corner of the workspace, select , and then select the offline form that you want to edit.

    The workspace for the offline form appears, displaying the fields of the offline form.

  3. For information on the selected offline form, select .

    The Form Information window appears.

  4. As needed, enter or modify the values in the Caption and Description boxes on the Form Information window.
  5. Select Update.

    The Offline form is saved.

Copyright © 2018 General Electric Company. All rights reserved.