Add an Offline Form

Steps

  1. Create an offline form.

  2. Select .

    The Offline Form Builder appears.

  3. Enter values in the Caption, Default ID, and Description boxes, and then select OK.

    Note: If you want your offline form to be the default offline form for this family, then select the Default check box.

    The offline form is created, and the list of available fields that can be added to the form appears.

  4. In the Available Fields pane, select the field that you want, and then drag it to the workspace for that offline form.

    The field is added to the workspace for that offline form.

  5. If you want to rearrange the fields for the offline form, then select and drag the items that you want to remove back to the Available Fields pane, and then select and drag the fields back to the workspace as needed.
  6. If you want to delete the fields in the offline form, then drag and drop fields from the datasheet back to the Available Fields pane as needed.
  7. Select .

    The offline form is saved.

 

Copyright © 2018 General Electric Company. All rights reserved.