Cognitive Analytics Workflow

This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.

  1. Create a query to return the historical records for your assets, stored in Work History or Equipment records.

    Tip: See the Cognitive Analytics Data Model.

  2. Create a cognition that will use the query to classify your data.
  3. Design the cognition, which includes adding nodes and connections that represent the inputs of historical data, logic, and outputs of classified data.

    Note: Interaction with the design canvas, such as adding and moving nodes, is not available on touch-screen devices.

  4. Activate the cognition.
  5. Execute the cognition or configure a schedule for cognition execution.
  6. Use the classified data that is produced by the cognition for metrics and additional analytics.

Copyright © 2018 General Electric Company. All rights reserved.