Cognition Records

Cognition records store basic information about cognitions. This topic provides an alphabetical list and description of the fields that exist for the Cognition family and appear on the Cognition datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Active? Boolean Indicates whether the cognition is active or inactive. Reflects the selection of the activate/deactivate policy button in the Details workspace. When Active? is true, the cognition will execute at the scheduled interval. When Active? is false, the cognition will not execute.
Classification Relationship Character The relationship family that links the input data source to the output family.

This field does not appear in the Details workspace by default.

If the family in the Output Family field is included in the relationship definition of the Has Classified Data relationship family, the Has Classified Data relationship family ID is populated automatically in this field. For all other families, this field remains empty.

Cognition Manual Start Date Date A date by which records from the input data can be filtered before cognition execution.

Contains the value that you specify in the Process Cognition data starting from this date box in the Details workspace.

If a cognition is executed manually and the query supplying the input data has a query prompt on a date field, the value in this field is passed as a date parameter, and the query will only return records that satisfy the query prompt's logic.

If a cognition is configured to be executed according to a schedule, on a successful execution, this field is populated automatically by the GE Digital APM system with the value in the Last Scheduled Execution field.

See the About Cognition Execution topic for more information.

Configuration

Text

Configuration information for the cognition.

This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.

IMPORTANT: Do not modify the contents of this field.

Data Input Character The reference to the data source (e.g., query) to be processed by the cognition.

Contains the data source that you specify in the Bulk Input Data box in the Details workspace.

The data structure found in the referenced data source provides the input fields to use when designing the cognition. Additionally, the data provided in the referenced data source is the data that will be processed when the cognition is executed.

Notes

  • The data source must include the Entity Key for the records.
  • Ensure that the query you use is a Select query. Other types of queries will cause errors to occur.
Description Text A description of the cognition. None
Last Scheduled Execution Date The end date for the scheduled execution of the cognition. This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.
Layout Text The design layout of the cognition.

This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.

IMPORTANT: Do not modify the contents of this field.

Name Character The name of the cognition. This field is required and must be unique.
Next Scheduled Execution Date The next date for a recurring scheduled execution of the cognition. This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APMM System.
Output Family Character The family to which the cognition will write classified data when executed.

Contains the name of the family that you select in the Classification Family box in the Details workspace.

The data structure found in the referenced family provides the output fields to use when designing the cognition.

Note: Only a family included in the relationship definition of the Has Classified Data relationship family and the same family that provides the data source in the Data Input field are available to be selected in this field.

Schedule Character Code defining the cognition's schedule. This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.
Schedule Executed Boolean Indicates whether or not the currently configured schedule has executed at least once. This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.
Schedule Time Zone Character The time zone associated with the scheduled execution of the cognition. Contains the time zone that you specify in the Time Zone box in the Edit Schedule window.
Scheduled Boolean Indicates whether or not the cognition has a defined execution schedule. This field does not appear in the Details workspace by default. This field is populated automatically by the GE Digital APM System.
Security Group Numeric Contains the security group that has privileges to modify the cognition.

This field contains the security group that you specify in the Security Group box in the Details workspace.

Copyright © 2018 General Electric Company. All rights reserved.