A Case node is a node that you can use in a cognition to set up scenarios in which the output values of the node are changed automatically based on specific input values. Throughout this documentation, we refer to each defined scenario as a Case.
Each Case within the Case node has one Case value and one output value. If the input value for the Case node matches a Case value, the GE Digital APM system will use the corresponding output value defined for that Case.
There are two types of Cases in the Case node, which we refer to as the If Case and the Default Case throughout this documentation:
Copyright © 2018 General Electric Company. All rights reserved.