Build SAP Plan from Actions

You can implement actions in ASM to manage their execution in GE Digital APM. Or, if you want to manage the execution in SAP, you can implement them in the Manage Actions section of ASI, as described in the following steps. Alternatively, you could create WMIs and link actions to WMIs manually. Or, you could import SAP objects into ASI as WMIs.

Steps

  1. Access an existing ASI package.
  2. Select the row containing the action to which you want to link an implementation method, and then select Build SAP Plan.

    The Select Action Mapping window appears.

  3. Select one of the following options:

  4. Select Build.

    The action(s) are now associated with WMI(s). Now, when this package is implemented, you can manage the action(s) in SAP.

Copyright © 2018 General Electric Company. All rights reserved.