Create a Work Management Item (WMI)

You can use the following the steps to create the work management items that will build out your implementation package.

Steps

  1. Access an existing ASI package.
  2. In the left pane, in the WMI tree for the package, select the parent item under which you want to add the new WMI.

    The datasheet for the selected WMI appears.

    Note: The options for which WMI types can be added depend on which node you have selected in the tree. Any WMI type can be added at the root node (i.e., the ASI Package tab).

  3. Select , and then select the WMI type that you want to add under the parent you selected.

    The datasheet for the new WMI appears.

  4. As needed, enter values in the available fields, and then select .

    The WMI is created and added to the package, and it appears in the WMI tree. The icon appears next to the WMI to signify that it was added since the package was last implemented.

Copyright © 2018 General Electric Company. All rights reserved.