The status of a Health Indicator record is based upon values that are stored in the Health Indicator record and the source records to which the Health Indicator record is linked. Each source record defines the upper and lower limit values that are compared to the most recent reading values in order to determine the status of a corresponding health indicator.
When viewing the Asset Health Manager page with an asset record selected in the Asset Hierarchy, a status icon appears next to each health indicator listed in the This Asset section and each asset listed in the Subsidiary Assets section.
The following icons are used to represent the various statuses of a health indicator.
Status | Icon | Description |
---|---|---|
Normal |
![]() |
Indicates that the corresponding Health Indicator record meets normal status criteria. |
Warning |
![]() |
Indicates that the corresponding Health Indicator record meets warning status criteria. |
Alert |
![]() |
Indicates that the corresponding Health Indicator record meets alert status criteria. |
No Readings |
![]()
|
Indicates that the health indicator source record of the corresponding Health Indicator record is not associated with any reading source records. For example, if the source record is a Measurement Location record, the status icon will be gray if the Measurement Location record is not linked to any Reading records. |
No limit values | No icon | For numeric health indicators, if limit values are not defined in a health indicator source record, no status will appear for the corresponding health indicator. |
When viewing the Asset Health Manager page with an asset record selected in the Asset Hierarchy, the This Asset section contains gauges showing the latest reading value stored in the Health Indicator record in respect to the corresponding limit values.
Each gauge contains various colored sections that represent the status criteria that the Health Indicator record could meet. The latest reading value is displayed on the gauge, along with a black pointer that identifies the status of the reading.
The gauge displays details differently depending on the limit values that are defined, the reading values that exist, and whether the health indicator has character or numeric readings. The following table summarizes these scenarios.
Scenario |
Reading Type |
Description |
Example Gauge |
---|---|---|---|
Latest reading falls within defined limits.
|
Numeric |
The latest reading is displayed proportionally to where the reading falls between the limit values. |
|
Character |
The latest reading is displayed in the center of the corresponding status section. |
|
|
Latest reading does not fall within defined limits. |
Numeric |
The latest reading is displayed with an arrow pointing off the gauge in the direction of the exceeded limit. |
|
Character |
The latest reading is displayed in the center of the green status section. |
|
|
A level 1 or 2 limit value is not defined for the health indicator.
|
Numeric |
The sections in a gauge are displayed based on the limit values that are defined. The latest reading is displayed proportionally in the corresponding section if the limit values provide enough information to determine the relative position of the reading, otherwise, the reading is displayed in the center of the corresponding section. |
|
Character |
The latest reading is displayed in the center of the corresponding status section. |
|
|
The health indicator has no reading values associated with it, but limits have been defined. |
Numeric |
The text No Readings is displayed in the gauge along with the defined limit values. |
|
Character |
The text No Readings is displayed in the gauge. |
|
|
The health indicator has reading values associated with it, but no limits have been defined. |
Numeric |
The latest reading is displayed in the gauge, but no limit values are shown. |
|
Character |
The latest reading is displayed in the center of the green status section. |
|
|
The health indicator has no reading values associated with it and no limits have been defined. |
Numeric |
The text No Readings is displayed in the gauge. |
|
Character |
The text No Readings is displayed in the gauge. |
|
Copyright © 2018 General Electric Company. All rights reserved.