About Health Indicator Sources

Health Indicator records are associated with health indicator source and reading source records that contain the limit values and reading values, respectively, that are compared to determine the status of the health indicator. One health indicator may exist for each health indicator source record associated with a piece of equipment. Reading source records are then used to provide the most recent reading value to the health indicator.

The following table summarizes the records that are configured as sources in the baseline GE Digital APM database.

Health indicator source record Corresponding reading source
GE Tag GE Tag Event records

Measurement Location

Reading records
OPC Tag

The most recent reading available from the OPC Server.

KPI KPI Measurement records

None (e.g., health indicators created via Policy Designer)

Health Indicator Value records

The following table summarizes the fields that define health indicator limit values for each of the baseline health indicator source records.

Health indicator source record Fields Containing Limit Values
GE Tag Upper and lower level limit fields in the GE Tag record.

Measurement Location

Upper and lower level limit fields in the Measurement Location record.
OPC Tag Upper and lower level limit fields in the OPC Tag record.
KPI

Target and Critical fields in the KPI Measurement record associated with the KPI record.

  • In KPI records where a low value is good, the Target value represents the upper level 1 limit and the Critical value represents the upper level 2 limit.
  • In KPI record where a high value is good, the Target value represents the lower level 1 limit and the Critical value represents the lower level 2 limit.
None Upper and lower level limit fields in the Health Indicator record.

The following table summarizes the fields in each reading source record that contain the latest reading value, which the Asset Health Indicator service copies into either the Last Numeric Reading Value or Last Char Reading Value field in corresponding Health Indicator records.

Reading source Field Containing Reading Value
GE Tag Event record Type

Reading record

Reading Value Character

Reading Value Numeric

Reading from the OPC Server

N/A

KPI Measurement record Actual
Health Indicator Value record Value (Numeric)

Copyright © 2018 General Electric Company. All rights reserved.