Map a Field to a Device Mapping

Steps

  1. Access the Device Mapping for the required device.
  2. In the Mappings workspace, select the Fields tab.

    The Fields section appears.

  3. In the Select APM Family box, select the family.

    Note: The Select APM Family box will only contain families that have been mapped to the selected device mapping.

  4. In the Select APM Field box, select the field.

    Note: The Select APM Field box will only contain fields of the family that was selected from the Select APM Family box.

  5. In the Select Calibrator Field box, select the calibrator field.
  6. As needed, select or clear the following check boxes:

  7. Select Save.

    The field is mapped to the device mapping.

Copyright © 2018 General Electric Company. All rights reserved.