Calibration Device Mapping Records

Calibration Device Mapping records store information about the fields that are defined in the Calibration Device Mapping family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the Calibration Device Mapping family and appear on the Calibration Device Mapping datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Device Driver ID Character The ID of the supported driver. This field does not appear on the datasheet and is auto populated with the ID of the selected supported driver.
Linked Mapping Character A value associated with the send mapping for the selected receive mapping.

This field is enabled when the value in the Mapping Direction field is Receive.

This list is filtered by the value that you select in the Template Type field.

This field is required.

Mapping Direction Character The type of direction of the outgoing data from GE Digital APM to a calibrator and incoming data from a calibrator to GE Digital APM.

This field appears a list and contains the following values:

  • Send
  • Receive

When you select Receive, the Linked Mapping field is enabled.

Mapping ID

Character

The ID of the device mapping

You can enter a value in this field. The value must be unique.

This field is required.

Mapping Query Character The query for sending data to a calibrator or receiving data from a calibrator. You must select a query that has been specified in the Queries folder.
Mapping Type Character The type of device mapping.

On the datasheet, this field appears as a list labeled Template Type and contains the following calibration templates:

  • Analog Calibration
  • Discrete Calibration
  • Functional Test

Depending on the selection, the Linked Mapping field is populated automatically.

Copyright © 2018 General Electric Company. All rights reserved.